Community Manager
Apr 24, 2022
10:48 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Apr 24, 2022
10:48 PM
AURIX™ MCU: QSPI pin configuration – KBA235129
Community Translation: AURIX™ MCU: QSPIピン設定 – KBA235129
Version: **
Queued synchronous peripheral interface (QSPI) functions as master or slave modes; depending on the mode selected, the pin configuration is as follows:
When the master mode is selected:
- MRSTxA to MRSTxH can be the input for the QSPIx
- MTSRx is the output of the QSPIx
When the slave mode is selected:
- MTSRxA to MTSRxH can be the input for the QSPIx
- MRSTx is the output of the QSPIx
For more details, see the “Queued Synchronous Peripheral Interface (QSPI)” section of the user manual.
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
- Tags:
- qspi
Rate this article: