Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: PWM resolution generated by GTM - KBA235553

AURIX™ MCU: PWM resolution generated by GTM - KBA235553

1000 replies posted First like given 750 replies posted
IFX_Publisher2
Community Manager
Community Manager
Community Manager

Community Translation: AURIX™ MCU: GTMによって生成されるPWM解像度 - KBA235553

Version: **

In AURIX™ TC2xx, the maximum GTM (Generic Timer Module) clock frequency is 100 MHz; therefore, the highest resolution can be 10 ns.

In AURIX™ TC3xx, the maximum GTM clock frequency is 200 MHz; therefore, the resolution is higher up to 5 ns.

Note:    This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series
0 Likes
290 Views