Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: Max number of analog input channels that can be measured simultaneously – KBA235329

AURIX™ MCU: Max number of analog input channels that can be measured simultaneously – KBA235329

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: AURIX™ MCU: 同時に測定できるアナログ入力チャネルの最大数 – KBA235329

Version: **

In the VADC module, one ADC converter has one dedicated Sample&Hold unit (no multiple S&H units).

Therefore, the maximum number of analog input channels that can be measured simultaneously is up to the maximum number of the AD converters implemented in the VADC module.

(For example, VADC of TC27x has eight AD converters. Therefore, up to eight analog input channels can be measured simultaneously.)

For more details, see the “Summary of Features” section in the datasheet.

Note:   This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series
0 Likes
174 Views