Community Manager

Community Manager
Aug 01, 2022
10:19 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
AURIX™ MCU: Manual configuration of AURIX™ Development Studio - KBA235950
Version: **
If the Auto-discover compiler include paths is disabled, right-click on the folder to quickly add or remove a folder from the compiler include paths. Select the required action under C/C++ Compiler Includes to add or remove the folder as shown in the following figure.
Alternatively, include paths can be manually edited by accessing the C/C++ Build / Settings.
- Right-click on the project and select Properties.
- Select C/C++ Build from the list and select Settings.
- In the Tools Settings tab, select TASKING C/C++ Compiler -> Include Paths.
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
Rate this article: