Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: How to identify pin/ball-specific parameters in the datasheet – KBA235364

AURIX™ MCU: How to identify pin/ball-specific parameters in the datasheet – KBA235364

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: AURIX™ MCU: データシートのピン/ボール特有のパラメータの定義の仕方 – KBA235364

Version: **

For pinning information, see the “Package and Pinning Definitions” section in the datasheet.
For each package (e.g., BGA516), each port has a separate table (e.g., “Port 00 Functions”) to list the functions available on that port.
In the table, the buffer type for each pin/ball is shown in the “Type” column with abbreviations defined in the table footnote.
For datasheet parameters related to the types, see the “Electrical Specification” section.

For example, in the TC290 / TC297 / TC298 / TC299 32-Bit Single-Chip Microcontroller datasheet:, see Table 2-1 for details of ball M6 in BGA516 package of TC299x. See the footnotes to determine the details.

BinduPriya_G_0-1653283739077.png

Based on the table:

1:

  • Type is MP/PU1/VEXT.

2:

  • MP = Pad class MP (5V/3.3V)
  • PU1 = With pull-up device connected during reset (PORST = 0)
  • Vx = Supply

For parameters related to the pad class “MP” and supply “VEXT”, see the “Electrical Specification” section of the datasheet. 

Note:     This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series
0 Likes
364 Views