Community Manager

Community Manager
Jul 24, 2022
11:20 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
AURIX™ MCU: How many channels of ADCs can be synchronized for a parallel conversion - KBA234996
Version: **
For a parallel conversion, up to four Analog-to-Digital Converter (ADC) in a synchronization group can be exactly synchronized.
In case of more than four ADCs, there are variations of each ADC start time with the range of a few cycle of analog clock (fADC). Therefore, they are almost synchronized, if the same ADC trigger source input to each ADCs.
For more details, refer to the “Versatile Analog-to-Digital Converter (VADC)” se
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
Rate this article: