Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: Generation of assembly files in AURIX™ Development Studio (ADS) – KBA235488

AURIX™ MCU: Generation of assembly files in AURIX™ Development Studio (ADS) – KBA235488

IFX_Publisher1
Community Manager
Community Manager
Community Manager
250 sign-ins First comment on KBA 250 replies posted

Community Translation: AURIX™ MCU : AURIX™ Development Studio (ADS)でのアセンブリファイルの生成 – KBA235488

Version: **

Follow these steps to generate the *.src files after a build in AURIX™ Development Studio:

  1. Create the makefile.targets file in the project root, with the following content:
    Screenshot (22).png

    Note: The white space before the command “find” must be a TAB, do not use white space.
  1. Left-click the project, choose Properties, select C/C++ Build, and then select the Behavior tab.
  2. Add the target saveobjects to the Build (Incremental build) list of targets, as shown in the following screenshot.

    MohammedA_41_2-1653559725828.png

    Figure 1

  3. Click Apply and Close. After a project build, the *.src files can be found in the Build folder with the extension *.src_bak (see Figure 2).

    MohammedA_41_3-1653559757290.png
    Figure 2

     

 

Note:

This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series

 

 

0 Likes
311 Views