Community Manager

Community Manager
Jun 27, 2022
05:49 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
AURIX™ MCU: Free tools for evaluation boards – KBA235619
Version: **
AURIX™ free tools are available on www.infineon.com/cms/en/tools/aurix-tools/free-tools webpage for the AURIX™ MCU evaluation boards.
- Use the AURIX™ Development Studio or the AURIX™ Free Tool Chain for editing, compiling, and debugging application code.
- Use the Infineon MemTool for flash programming.
To get application running:
The AURIX™ evaluation boards have an onboard debugger which enables the usage of the device access server (DAS) as a tool connection. Using DAS, users can halt the program execution, trigger resets, read/write in the address space or use the multi-core debug solution (MCDS) trace viewer, which is a non-intrusive tool that helps to identify time-sensitive bugs.
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
Rate this article: