Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: Ethernet packet filtering - KBA236051

AURIX™ MCU: Ethernet packet filtering - KBA236051

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: AURIX™ MCU:イーサネットパケットフィルタリング - KBA236051

Version: **

Question: What types of packet filtering are supported by the Gigabit Ethernet (GETH) MAC of the AURIX™ TC3xx?

Answer:

The AURIX™ TC3xx GETH module supports packet filtering based on Source MAC address, Destination MAC address and Virtual Local Area Network (VLAN) tag of the received packets. The received packets can either be filtered based on a precise match or a range-based match.

Note: This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC3xx series

 

0 Likes
114 Views