Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: Device Access Server (DAS) – KBA235789

AURIX™ MCU: Device Access Server (DAS) – KBA235789

IFX_Publisher1
Community Manager
Community Manager
Community Manager
250 sign-ins First comment on KBA 250 replies posted

Version: **

The Device Access Server is an abstraction of the physical connection and is used to enable the connection to AURIX™ devices using different interfaces like JTAG or DAP. DAS is used with all the AURIX™ evaluation boards such as lite kit, application kit, or triboard.

The DAS installation provides several tools like:

  • DAS Device Scanner: It is used to check that the board is properly detected by the computer and trigger simple operations such as reset, reset and halt, reading the device information, or read/write data from/to the device
  • DAS Perfmeter: You can measure performance parameters such as the number of transactions executed per second
  • MCD Basic Client: You can open one instance per core, set breakpoints and execute operations like run, stop or step
  • MCDS Trace Viewer: It is a tool used for tracing such as instruction, compact function, or data logging

For more details on the DAS tool interface, see the DAS webpage.

Note: This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series
0 Likes
659 Views