Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: Creating a library project in AURIX™ Development Studio - KBA235854

AURIX™ MCU: Creating a library project in AURIX™ Development Studio - KBA235854

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: AURIX™ MCU: AURIX™ Development Studio でのライブラリ プロジェクトの作成 - KBA235854

Version: **

To create a library project in AURIX™ Development Studio, do the following:

  1. Click File > New > New AURIX™ Project from the AURIX™ Development Studio toolbar as Figure 1 shows.
BinduPriya_G_5-1659417027177.png

 

Figure 1     Selecting New AURIX™ Project

  1. Select Infineon > New AURIX™ Library Project > Next from the New Project window as Figure 2 shows.

 

BinduPriya_G_4-1659416957761.png
Figure 2     Selecting New AURIX™ Library Project

  1. Follow the wizard steps, to select the project name and the target device as shown in Figure 3 and Figure 4 respectively.
BinduPriya_G_3-1659416874839.png
Figure 3   Selecting the Project name
 
BinduPriya_G_1-1659416787754.png

 

Figure 4   Selecting the target Device

  1. By default, AURIX™ Development Studio creates an empty library project with a static library archive (.a file) as Figure 5 shows, which can be filled with the decided content.
BinduPriya_G_0-1659416706555.png

Figure 5    Library project

383 Views