Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: Configure an external GCC toolchain in AURIX™ Development Studio (ADS) - KBA235472

AURIX™ MCU: Configure an external GCC toolchain in AURIX™ Development Studio (ADS) - KBA235472

IFX_Publisher1
Community Manager
Community Manager
Community Manager
250 sign-ins First comment on KBA 250 replies posted

Version: **

To configure an external GCC toolchain, follow these steps:

  1. Activate the build configuration.
    Right-click the project and do one of the following (see
    Figure 1)
  • Select Build Configurations>Set Active> 2 External GCC - Debug.
  • Select Build Configurations>Set Active> 3 External GCC - Release.

    Screenshot (24).png

    Figure 1 Activate the build configuration

The selected configuration is now active.

  1. Click Active Project Properties.
    Screenshot (25).png
    Figure 2 Active Project Properties

The Settings window appears.

  1. Populate the fields Prefix and Path (see Figure 3).
    The path will be the bin folder of a valid GCC TriCore™ compiler installation.
    The prefix will correspond with the prefix of the tool name. For example, if the gcc executable name is tricore-gcc.exe, the prefix will be tricore-.

    Screenshot (26).png
    Figure 3 Prefix and Path fields
  1. Click Apply and Close. The toolchain is now configured and ready to build the project.

Note: 

This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series
0 Likes
917 Views