Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: CHIPID and JTAGID – KBA235686

AURIX™ MCU: CHIPID and JTAGID – KBA235686

IFX_Publisher2
Community Manager
Community Manager
Community Manager
25 likes received 1000 replies posted First like given

Community Translation: AURIX™MCU:CHIPIDおよびJTAGID – KBA235686

Version: **

In AURIX™ MCU, the CHIPID and JTAG ID registers identify the device and user’s board.

CHIPID

The CHIPID register helps the user to identify the following characteristics of the device such as:

  • The device series
  • The package classes
  • The additional features such as the hardware security module or emulation
  • The flash memory size
  • The different variants based on temperature range or frequency
  • The version of the flash microcode

JTAGID

Tools use the JTAGID register to adapt their behavior when connecting to the device. It identifies the proper register mapping or enables additional modules (e.g., multi-core debug solution (MCDS)).

Note:    These two registers offer different information.

Note:   This KBA applies to the following series of AURIX™ MCUs

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series
0 Likes
298 Views