AURIX™ MCU: Accessing files history in AURIX™ Development Studio – KBA235952
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Community Translation: AURIX™ MCU: AURIX™ Development Studio でのファイル履歴へのアクセス – KBA235952
Version: **
In the AURIX™ Development Studio (ADS), it is possible to replace the current version of files with an older one by browsing through the local history.
This feature is inherited by Eclipse™. Right-click on a file and select Replace With > Local History... as shown in the figure below to replace the content of the file.
Use Compare With feature to compare older versions when it is not needed to replace the content of the file.
By accessing the Local History, a compare window appears from which the revision time can be selected. Double-click on the revision time, a compare viewer window of the two versions of the file is displayed. The changes can be replaced by clicking on the Replace button.
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
- Tags:
- ide