Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AC Rating of LX5V Pin of S6BP501A and S6BP502A - KBA227095

AC Rating of LX5V Pin of S6BP501A and S6BP502A - KBA227095

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: AtsushiT_61           Version: **

Translation - Japanese: S6BP501AおよびS6BP502AのLX5VピンのAC定格 - KBA227095 - Community Translated (JA)

Question:

What is the AC rating of LX5V pin of S6BP501A and S6BP502A?

Answer:

Figure 1 shows an example of the switching waveform of the LX5V pin of S6BP501A and S6BP502A.

Figure 1. Example of LX5V Switching Waveform

pastedImage_0.png

Since the AC withstand voltage of the LX5V pin is 12 V, IC will not be damaged even if a ringing waveform as shown in Figure 1 occurs.

To measure the high frequency ringing waveform correctly, measure close to the IC pin. Also, it is necessary to connect the oscilloscope probe GND short, as shown in Figure 2.

Figure 2. Oscilloscope Probe GND

Capture.JPG

A method to reduce ringing noise is to add a snubber circuit. Figure 3 shows an example of a snubber circuit.

Figure 3. Example of a Snubber Circuit for DD5V

pastedImage_18.png

                                     

0 Likes
348 Views
Contributors