8 Mb and 16 Mb Excelon F-RAM ECC Implementation – KBA232933
Community Manager
Jun 23, 2021
11:10 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jun 23, 2021
11:10 PM
Community Translation: 8 Mbおよび16 Mb Excelon F-RAM ECCの実装 – KBA232933
Version: **
Question: Are there any differences in the ECC implementation between the existing Excelon™ and the new 8 Mb and 16 Mb Excelon products?
Answer: Excelon 8 Mb and16 Mb devices implement 2-bit error correction and 3-bit error detection, while the earlier low-density Excelon devices including legacy F-RAMs implement 1-bit error correction and 2-bit error detection.
- Tags:
- 16 Mb
- 24 FBGA
- 2bit correction
- 2Mb
- 3 bit detection
- 4Mb
- 8EIAJ
- 8GQFN
- 8Mb
- block erase
- drop in replacement
- ecc
- excelon
- f-ram
- fbga
- field
- high performance
- memories
- spi
Rate this article: