Intelligent Power Modules (IPM) Forum Discussions
hello authorized
I use this IPM (IKCM20R60GD). I found another app note. I saw ITRIP PIN.I saw how this pin was used. Can I follow the same steps in this integrated?
Can you send me documents related to this integration that I can use?
Thank for your concern.
Show Less
hello authorized
I use this IPM (IKCM20R60GD). I found another app note. I saw ITRIP PIN.I saw how this pin was used. Can I follow the same steps in this integrated?
Can you send me documents related to this integration that I can use?
Thank for your concern.
ex. Voc/Ipeakofdevice ,this formula and more
Show LessHello,
there is this image:
In which a IM828-XCC is used in order to convert an AC source, while correcting the power factor.
Do you have any sample about that? (some code for the microcontroller, or some evaluation board)
Kind regards,
Marco Negrini
Show Less知乎粉丝在一篇回答下面问的问题:有没有Si IGBT+SiC 二极管的IPM啊
回答链接为:https://www.zhihu.com/question/355286254/answer/968098837
麻烦工程师解答~谢谢!😀
Show LessHi,
I am using imc101t-F048 along with my custom board based on Eval-IM535 to drive my compressor using IMOTION Solution designer although the compressor is working but it is consuming more current then normal can you please help in this regard which parameters affect current consumption. I have attached the Compressor file and IMOTION file.
Thanks, and Regards
Hassan Ishtiaq Minhas
Show Less您好,我们需要使用IKCM30F60GA来替换IRAMX16UP60A(原),且替换场景为基于IRAMX16UP60A的已经设计好板子上,我们所要做的工作是通过转接板来进行芯片的替换。我们现在有几个问题不能确认。
1:IKCM30F60GA的散热能力是否比IRAMX16UP60A要好,他的应用场景在地铁门的电机上,所以我们需要比较好的散热。
2:IKCM30F60GA的芯片引脚比IRAMX16UP60A要多出VS(U\V\W)这三个,我们把这三个直接接到电机的UVW侧,是否会对电机产生影响?我们需不需要在转接板上增加电容?
谢谢您的回答。
Show Less
Hi Sir,
Good day.
I am testing Motor Driver - IMM101T-046M, Three Leg Shunt using MCU to control ON/OFF and Speed.
I could turn on & control speed of motor by applying Pin 34, VSP pin with spinning forward direction .
But when I want to control the motor turn to reverse direction, using Pin4, P1.7 , the motor still spin same forward.
Could I know how to set in MCE Wizard & Firmware programming on MCU, so that the motor can turn Reverse Direction.
Pls advise. Thanks.
Show LessHi
i am using Eval-IM535 board to drive a compressor using IMOTION solution designer but due to some weird reason as soon as i turned on the compressor it starts for few seconds and reached 700 RPM and then stops suddenly during this time i have checked my power supply which detects sudden decrease in voltage i.e. from 307V to 25V. Can you please help in this regard.
Thanks
Hassan Ishtiaq Minhas
Show LessI have designed IPM 535 U6D based Board but it is not available in the market.
Due to this reason i am looking for its replacement i have found IKCM30F60GD as a replacement.
Can you please confirm if both of them are pin to pin compatible?
If no what are the changes required to make it compatible?
Thanks
Hassan Ishtiaq
Show Less