- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I have a Mitsubishi power IGBT module having a max current of 800 A, peak current of 1600 A, and total gate charge of 4500 nC. I am planning to use an infineon 1ed020I12-f2 driver. I am going to use a bipolar supply of +15 and -8 volts. The application controls a Motor with the IGBT Grounding the motor to energize it. It is an On Off type of operation in which the motor will be activated 1 to 3 times per second then will be inactive for perhaps a second. It seems from the datasheet That this particular chip can handle this. Is that correct? Also, my impressions is that the clamp output is not necessary when using a bipolar drive. Is this also correct?
Thank you
Jeff
Solved! Go to Solution.
- Labels:
-
IGBT
- Tags:
- driving igbt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @jeffluminais,
As per the device datasheet peak gate current requirement is > 4.5A. I would recommend you to go ahead with 1EDI60I12AF
Thanks & Regards,
Rishabh
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
Hello @jeffluminais ,
There is no data for the internal gate resistance of the module in the datasheet. Should it be taken as 0?. Please confirm.
Thanks & Regards,
Rishabh
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
Hello @jeffluminais,
As per the device datasheet peak gate current requirement is > 4.5A. I would recommend you to go ahead with 1EDI60I12AF
Thanks & Regards,
Rishabh