Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

IGBT Forum Discussions

answerlishen
IGBT
Hi,I want to measure the Vce(on) of IGBT, I have found one chip can achieve my goal; it's IR25750LTRPBF, but it's a Discontinued Product. Since 2019 i... Show More
Ahmed_495
IGBT
Hello, I am trying to use your IKW15N120T2 IGBT in my work for showing the effect of different design approaches on IGBT lifetime. I want to use the m... Show More
MS_19060803
IGBT
Hi all, We are considering the use of the following products. ・FF600R12ME4_B73 ・FF600R12ME4P_B72 ・FF600R12ME4W_B73 ・FF600R12ME4_B72  I have a question... Show More
ASW
IGBT
Hi I have a question of IGBT current. 3 IGBTs are specified in FZ2400R17HP4_B9 schematic. Is Icnom(2400A) current for one IGBT? Show More
SiCk
IGBT

在IGBT寿命预测过程中,需要利用IGBT加速老化试验的老化数据和寿命数据信息提出IGBT寿命预测方法。

Sriram_07
IGBT
Hello,  We are using FS200R07PE4 igbt module for EV motor controller application. While testing the igbt module it suddenly stopped working . DC termi... Show More
SiCk
IGBT

Hi Infineon, are there SiC IGBT devices on the official website? If so, where can I inquire?

Emily
IGBT

Do Infineon have FS03MR12A6MA1LB Power Module Cooling System ? (for testing Rth)

(AN-HPDPERF-ASSEMBLY)

Anwaar_E_Rasool
IGBT
IR2136S
solved msg Solved
Hi, I'm using IR2136 to run a BLDC (over 300V) with XNF15N60T IGBTs. I'm using 3.3V logic by an ESP32 controller for all 6 phase controls. Enable is p... Show More
NoamRabin
IGBT
Hello, I am using as a reference Infineon 22kw inverter power board schematics and I think i found an error: On page 11 named current sensors (page 13... Show More
Forum Information

IGBT

Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.