Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

IGBT Forum Discussions

liujianhua
IGBT
Three-level NPC2 topology, two horizontal tubes use FF2400RB12IP7, two vertical tubes use FF1800R17IP5, DC voltage 750V, AC side current 1050A, how to... Show More
BojanK
IGBT
We received Infineon’s IGBT modules - PN  FS200R06KE3BOSA1 , from a Chinese supplier. We opened the IGBT and there is quite big visual difference betw... Show More
liujianhua
IGBT
The npc2 converter adopts two different types of IGBT devices with horizontal and vertical tubes. How to analyze the device loss on the official websi... Show More
BMArmstrong
IGBT
Hi there, I am a bit new working with IPOSIM, and was trying to set up some specific parameters to calculate values for my heatsink needed. I am using... Show More
pclinh2001
IGBT
HelloAccording to some Infineon documentation when designing hardware for IGBT driver, there should be more capacitors between VCC - COM pins, and VCC... Show More
pclinh2001
IGBT
I am having difficulty in calculating Bootstrap capacitor values for IR2136 and IHW20N120R5 in the document provided by infineon (picture attached bel... Show More
Audiomatic
IGBT
Hello, I have a servo motor amplifier for a robot that I am trying to repair that has six (now obsolete) International Rectifier IRG4PC40UD IGBT’s dri... Show More
Mostafa
IGBT
I was wondering if there is any detailed life cycle assessment executed by Infineon and can be published for any of the IGBT technologies.  If so, is ... Show More
PeterAshraf
IGBT
Can someone suggest a replacement for the IGBT (Type SKB10N60A, Marking-K10N60) because the Infineon company does not produce it any more but to be wi... Show More
Forum Information

IGBT

Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.