Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

IGBT Forum Discussions

hello110300509
IGBT
Hello, I purchased IM818LCC and applied a bus voltage of 100-400V to it, providing a switch signal (5V). However, the module still cannot switch. What... Show More
Chileshe
IGBT
Application note AN2019-10 has an Inverter Welding Schematic however, some details are not clearly visible as the attached image is showing.  Could I ... Show More
sunder3069
IGBT

 

We require reference design for 50KW EV chargers is it available 

 

 

59e
IGBT
我在IPOSIM中使用了DC/DC巴克仿真,但运行后没有结果。不过我之前使用的时候没有遇到过这个问题。这是什么原因呢? Show More
Chileshe
IGBT
Hello. The AN2019-10 and AN2018-23 application notes have Inverter welding schematics which do not indicate the IC part number for driving IGBT gates.... Show More
saito
IGBT
Dear Sir or Madam, I am using FF150R12RT4 in our product.Please provide RoHS Certificate(2011/65/EU, (EU)2015/863) for FF150R12RT4. Thanks. Show More
ufuksfk
IGBT
Hello to All, I would like to ask Infenion Application Engineers about the PFC Inductor in that EVAL board: https://www.infineon.com/cms/en/product/evaluation-boards/eval-pfc5kikwwr5sys/... Show More
WANG_365
IGBT
The IGBT junction or case temperature is calculated with Foster model, the input parameters are  power losses, thermal data, et al. The loss and tempe... Show More
ABK
IGBT
Hi, We are currently trying to reduce the switching losses of a FS200R12KT4R IGBT module, to increase the power level of a 3 phase 2-level inverter. T... Show More
Rubacava
IGBT
I am designing a circuit to drive an igbt using 1ED3890MC12M.    Problem is when I first connect driver to pcb, I could connect to it for couple secon... Show More
Forum Information

IGBT

Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.