IGBT Forum Discussions
粉丝在知乎这篇文章下面问了这个问题:车规的igbt产品中,有用到RC-IGBT技术么?
文章链接:https://www.zhihu.com/question/532485914/answer/3186153078
希望有工程师帮忙解答😀
Show Less粉丝在英飞凌知乎发的这篇文章问了这个问题:为什么不直接根据测试数据积分呢,还要分段线性拟合
文章链接是:https://zhuanlan.zhihu.com/p/601848748#comment-10660961166?notificationId=1678688043664601088
希望有工程师能够帮忙解答~感谢😀
Show LessHello,
I am building a high voltage inverter operating at 200v. i am using isolated gate drivers and the supply for the gate drivers (15V) is also isolated. But the inverter switching causes a voltage spike in the gate driver power supply . the spike is happening at 40khz which is twice the switching frequency of the inverter. I have dc link capacitors and mlcc filtercaps attached to the dc line
Can someone help me figure out why the inverter switching noise is propagating to the low voltage side.
Thank you
CE间电压随着集电极电流上升而线性上升,这个区域称为饱和区
线性增加,那不应该叫做线性区吗?
到了所谓的退饱和区,电流饱和了啊,反而不叫饱和区了,这不是很奇怪吗?
你们是怎么定义饱和这个概念的?
知乎粉丝在这篇回答下面问的问题,希望有工程师帮忙回答~
Show Less
The IGW75N65H5_L2 Spice model does not function in LTSPICE, giving the error "Unknown subcircuit called in: xu4 n030 n033 n034 igw75n65h5_l2 tj=27"
The application notes (https://www.infineon.com/dgdl/Infineon-AN_2020_17_Simulation_models_of_IGBTs_and_power_silicon_diodes-ApplicationNotes-v01_02-EN.pdf) for this spice model seems to suggest it is compatible with LTSPICE.
Any help would be appreciated.
Can you help me see if this is normal? Is this pin condition caused by the electroplating process? Or was it renovated?
IRG4PC50UDPBF DC 10+
Show Less
Bonjour,
je souhaiterais savoir si le IHW30N160R5 est un bon équivalent du IHW30N160R2 ?
Merci.
Show Less