IGBT Forum Discussions
Sort by:
IGBT
Dear Infineon,
I am wondering what is partial discharge and how should this be considered in inverter applications? Thanks
I am wondering what is partial discharge and how should this be considered in inverter applications? Thanks
IGBT
Miller plateau
Solved
IGBT
Select models: FF300R12ME4 and FF300R17ME4. Intend to use the IGBT internal NTC resistor as the overheat protection sampling. What temperature is appr...
Show More
Select models: FF300R12ME4 and FF300R17ME4. Intend to use the IGBT internal NTC resistor as the overheat protection sampling. What temperature is appropriate for the overheat protection setting?
选用型å·ï¼šff300r12me4å’Œff300r17me4. 打算使用igbt内部的ntc电阻作为过çƒä¿ 护 é‡‡æ ·ï¼Œè¿‡çƒä¿æŠ¤ç‚¹è®¾ç½®åˆ°å¤šå°‘æ¸©åº¦åˆ é€‚ ? Show Less
选用型å·ï¼šff300r12me4å’Œff300r17me4. 打算使用igbt内部的ntc电阻作为过çƒä¿ 护 é‡‡æ ·ï¼Œè¿‡çƒä¿æŠ¤ç‚¹è®¾ç½®åˆ°å¤šå°‘æ¸©åº¦åˆ é€‚ ? Show Less
IGBT
IGBT
Original or facke?
Solved
Здравствуйте, коллеги. Подскажите, пожалуйста как можно проверить модули от поставщиков на оригинальность?Есть ли возможность пробить номер на сайте, ...
Show More
Здравствуйте, коллеги.
Подскажите, пожалуйста как можно проверить модули от поставщиков на оригинальность?
Есть ли возможность пробить номер на сайте, чтобы узнать действительно ли такой модуль выпускался на производстве Infineon?
Где можно найти информацию по этой теме? Show Less
Подскажите, пожалуйста как можно проверить модули от поставщиков на оригинальность?
Есть ли возможность пробить номер на сайте, чтобы узнать действительно ли такой модуль выпускался на производстве Infineon?
Где можно найти информацию по этой теме? Show Less
IGBT
Project: Battery Pack Testing System (900kW) Output voltage: 1300~1500V Please recommend suitable IGBT module I need 2500V IGBT module, current: 3...
Show More
Project: Battery Pack Testing System (900kW)
Output voltage: 1300~1500V
Please recommend suitable IGBT module
I need 2500V IGBT module, current: 300A,400A,600A,1000A. Infineon does not have such products, do you recommend choosing 3300V IGBT module products? Or is a three-level IGBT module suitable for this project? Show Less
Output voltage: 1300~1500V
Please recommend suitable IGBT module
I need 2500V IGBT module, current: 300A,400A,600A,1000A. Infineon does not have such products, do you recommend choosing 3300V IGBT module products? Or is a three-level IGBT module suitable for this project? Show Less
IGBT
Thermal Resistance
Solved
Dear Communities
Regarding IGBT Discretes,
What standard is Rthjc of IGBT based upon?
Thanks
BR
Regarding IGBT Discretes,
What standard is Rthjc of IGBT based upon?
Thanks
BR
IGBT
RC IGBTs vs. standard
Solved
Dears,I have read in the web about reverse conducting IGBTs. Could you please explain what are the difference with respect a standard IGBT and in whic...
Show More
Dears,
I have read in the web about reverse conducting IGBTs. Could you please explain what are the difference with respect a standard IGBT and in which application it can be used?
Thanks and best regards,
MaxP Show Less
I have read in the web about reverse conducting IGBTs. Could you please explain what are the difference with respect a standard IGBT and in which application it can be used?
Thanks and best regards,
MaxP Show Less
IGBT
motor drives
Solved
Hi Infineon team,
What is the root cause of the dV/dT limitation in motor drives?
Thanks, BR
What is the root cause of the dV/dT limitation in motor drives?
Thanks, BR
IGBT
Hello, Why does the collector current at high temperature get lower than that at low temperature after a certain value of V_GE? For instance, as shown...
Show More
Hello,
Why does the collector current at high temperature get lower than that at low temperature after a certain value of V_GE?
For instance, as shown in the transfer characteristic curve, Ic, at V_GE below 7.5V, is higher at 150°C than at 25°C. While as V_GE goes above 7.5V 150°C curve has lower Ic value than the 25°C curve.

Thank you! Show Less
Why does the collector current at high temperature get lower than that at low temperature after a certain value of V_GE?
For instance, as shown in the transfer characteristic curve, Ic, at V_GE below 7.5V, is higher at 150°C than at 25°C. While as V_GE goes above 7.5V 150°C curve has lower Ic value than the 25°C curve.
Thank you! Show Less
Forum Information
IGBT
Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.
Important links
Overview
Products
Simulation