Recent discussions
Sort by:
IGBT
We are using IGBT module f4-75r06w1e3 for a three phase inverter application. Wehave well tested gate driver based on IR2110 wich is isolated by VO312...
Show More
We are using IGBT module f4-75r06w1e3 for a three phase inverter application. We
have well tested gate driver based on IR2110 wich is isolated by VO3120 opto isolator. H bridge has RCD clamping snubber as well. it works properly at our full load condition with out transformer at
the output. When we connect the transformer at the AC output our module getting damaged. Can you please help me
to track the issue? Show Less
have well tested gate driver based on IR2110 wich is isolated by VO3120 opto isolator. H bridge has RCD clamping snubber as well. it works properly at our full load condition with out transformer at
the output. When we connect the transformer at the AC output our module getting damaged. Can you please help me
to track the issue? Show Less
IGBT
Fz1200r12kf5
Solved
Good day!Our company was acquired IGBT modules FZ1200R12KF5 to set the frequency converter Siemens SIMOVERT MASTER DRIVE but we suspect that these mod...
Show More
Good day!
Our company was acquired IGBT modules FZ1200R12KF5 to set the frequency converter Siemens SIMOVERT MASTER DRIVE but we suspect that these modules are fake. Is it possible to independently determine the authenticity of modules FZ1200R12KF5?
Thank you. Show Less
Our company was acquired IGBT modules FZ1200R12KF5 to set the frequency converter Siemens SIMOVERT MASTER DRIVE but we suspect that these modules are fake. Is it possible to independently determine the authenticity of modules FZ1200R12KF5?
Thank you. Show Less
IGBT
F3L400R12PT4_B26 3D model
Solved
IGBT
Pspice model problems
Solved
Hi, I'm trying to simulate the IKW40N120H3 IGBT using Capture/PSpice 16.5, and I get the following error message ERROR(ORPSIM-15108): Subcircuit L4XXX...
Show More
Hi,
I'm trying to simulate the IKW40N120H3 IGBT using Capture/PSpice 16.5, and I get the following error message
ERROR(ORPSIM-15108): Subcircuit L4XXXB_Lh3 used by X_Z1.XDIO is undefinedd
I've add the IFX_N120H3.lib into the simulation profile as a global library.
I'm not sure where the problem can be.
Thanks Show Less
I'm trying to simulate the IKW40N120H3 IGBT using Capture/PSpice 16.5, and I get the following error message
ERROR(ORPSIM-15108): Subcircuit L4XXXB_Lh3 used by X_Z1.XDIO is undefinedd
I've add the IFX_N120H3.lib into the simulation profile as a global library.
I'm not sure where the problem can be.
Thanks Show Less
- « Previous
- Next »
Forum Information
IGBT
Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.
Important links
Overview
Products
Simulation
Trending discussions