IGBT Forum Discussions
I have purchased F415MR12W2M1B76 MOSFET Power module. I need to know what kinds of connectors will be used for its connections. Will I have to made by myself or is there any recommended connectors that I may use for making connections gate driver circuit and output and input power supply.
Show LessWhen IGBT is turned on, many waveforms will have the gate pulled down. This is why
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IGBT%E5%BC%80%E5%90%AF%E6%97%B6%E6%A0%85%E6%9E%81%E8%A2%AB%E4%B8%8B%E6%8B%89/td-p/676960
Show Less大家有没有用过300A的mosfet,比如IPT012N08N5ATMA1,额定内阻1.2mΩ,在通电过程中实际上内阻会随着温升增加而变化,导致根据内阻测量电流会有偏差,请问有没有办法得到该片子随温度变化的内阻变化曲线?
The FF500R17KE4 device is planned to be used. The dead time of the device needs to be calculated, but there is no switching time curve in the sample. Please provide the recommended dead time for system applications and the switching time curve.
It is planned to be used in LLC circuits. The current during switching is small, about 20A, and the bus voltage is 1100V.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/FF500R12KE7%E5%BC%80%E9%80%9A%E5%85%B3%E6%96%AD%E6%97%B6%E9%97%B4/td-p/679828
Show LessI need a driver for an electric motor
We estimate that the voltage will be around 300 volts and 30-40Amps
I think we will need 4 IGBTS or mosfets around 2500 W each ( 4 phase )
The driver must have input from encoder.
I would like to have a suggestion for IGBT or Mosfet with matching gate drivers
If you need more information let us know
Thanks,
Anton
Show Less
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/%E5%85%B3%E4%BA%8EIKW40T120/td-p/678913
Show Less1. Input voltage 380V AC, output 700V, power 50KW, two tubes connected in parallel, switching frequency 36kHz, air cooling; 2. How to calculate tube loss to select the corresponding Infineon tube; 3. To verify whether the calculation is correct, IPOSIM simulation verifies whether the loss is consistent with the calculated loss; 4. The project is in the pre-research and selection stage; please help and support, thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/I%E5%9E%8BNPC%E4%B8%89%E7%94%B5%E5%B9%B3%E7%AE%A1%E5%AD%90%E9%80%89%E5%9E%8B%E8%AE%A1%E7%AE%97%E4%B8%8E%E4%BB%BF%E7%9C%9F/td-p/678603
Show LessI bought two devices, IM818-SCC and IM818-LCC. Their current values don't work. How can I tell the difference when soldering to the board? The screen printing completely blocked the board. Can I measure the IGBT body diode scc 0.510V LCC0.471V as a basis?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/im818%E7%94%B5%E6%B5%81%E5%80%BC%E6%B5%8B%E9%87%8F/td-p/678689
Show LessThe TLE8366EV50XUMA1 we ordered, but the actual delivery label is TLE8366EV50. According to the information on the official website, XUMA1 has a specific meaning, but currently the Material Content Sheet on the official website is MA#: MA003502968, and the actual product label also shows this MA #,这个MA #我看都符合XUMA1所标识的要求呀, so I'm not sure about TLE8366EV50 and What's the difference between TLE8366EV50XUMA1? Which model do we take as the basis for the actual order?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/TLE8366EV50XUMA1-%E5%92%8CTLE8366EV50%E7%9A%84%E5%8C%BA%E5%88%AB/td-p/677369
Show Less