IGBT Forum Discussions
Hello. - Hi! May I ask
1. what is inside the green schematic module (UNDER_VOL_DET ECT ION) in Figure 33? Is it the part of the linear regulator in the lower left corner of Figure 39?
2. What exactly is the purpose of the 0-ohm resistor R136 connected to IC4 pin 6 in Figure 39?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IGBT%E9%A9%B1%E5%8A%A8/td-p/690458
Show LessHello, I need a driver board from the Hybrid Kit for HybridPACK™ 1 Evaluation Kit for Applications with HybridPACK™ 1 Module Kit. Can you provide me with the schematic and PCB for this board?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IGBT%E9%A9%B1%E5%8A%A8%E6%9D%BF%E5%8E%9F%E7%90%86%E5%9B%BE%E5%92%8CPCB/td-p/684385
Show LessWhat is the difference between your 1ED010I12-FA, 1ED010I12-FTA, 1ED010I12-FA2 chips and can they replace each other?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IBGT%E6%A0%85%E6%9E%81%E9%A9%B1%E5%8A%A8%E8%8A%AF%E7%89%87%E9%80%89%E6%8B%A9/td-p/687131
Show LessHello.1 May I ask if the capacitors and resistors (e.g. C79 and R82) in parallel between the gate and emitter of the IGBT in Figure 38 in the attachment are structures in the IGBT module or on the driver board?
2. Is the transient suppression diode D3_UB and the diode below it, back-to-back with it, in figure 37 an active clamp circuit? And what is the purpose of R28_UB and D6_UB?
3. What is the function of Schottky diodes D5_UB and D4_UB?
4 For beginners who want to learn this driver board, does Infineon provide any other learning materials or suggestions (e.g. schematic library and PCB library for this board)?
I'm looking forward to hearing from you.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IGBT%E9%A9%B1%E5%8A%A8/td-p/689041
Show LessLet me know "IGBT Auirg4ph50s Short circuit withstand WITHSTAND TIME ".
I can't find it in datasheet.