IGBT Forum Discussions
When doing the experiment, the inter-ge voltage of the IGBT will start to oscillate as the inter-ce voltage increases, what are the possible reasons for this phenomenon?The PCB board has only the basic signal inputs, opto-coupler isolation, drive resistor and IGBT.The blue waveform in the picture is the inter-ge voltage and the green waveform is the inter-ce voltage.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IGBT%E5%AF%BC%E9%80%9A%E6%97%B6VGE%E6%B3%A2%E5%BD%A2%E9%9C%87%E8%8D%A1/td-p/695833
Show LessFF600R12ME7_B11英飞凌此款芯片,三管并联组成的逆变器,在整机上测量续流二极管压降正常0.381V,但是IGBT测量击穿压降在1.3-1.4V,拆下来以后再测量IGBT没有击穿,压降无穷大,请问这是什么原因?现场条件是每一个IGBT正负之间并联了一个吸收电容,大约在2UF左右,测量点也是在紧靠IGBT模块引脚输出点位,输出带电抗器,不知是什么原因真是奇怪了?和母线电容有关系吗?是对母线电容充电造成的吗?还是其他什么原因?
Show Less1 &3. This development board has been discontinued due to design issues and is no longer available for sale, and we do not recommend any further reference to its related design, please understand.
2. Q4 is a PMOS, which serves as an anti-reverse connection protection circuit. Its gate is connected to a resistor to ground, and if a forward voltage is connected to the input, current flows through the body diode of the PMOS to the load side. If the forward voltage exceeds the voltage threshold of the PMOS, the channel conducts. This reduces the drain-source voltage ( VDS ) of the PMOS, which reduces power consumption. A voltage regulator, BZV55-C13, is typically connected between the gate and source to prevent an overvoltage condition at the gate-source voltage ( VGS ) and also to protect the PMOS from breakdown during input power fluctuations.
This board was released in '12, and now that the technology iteration of power supply design solutions is so rapid, it makes little sense to continue to reference a faulty board.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E6%99%BA%E8%83%BD%E7%94%B5%E6%BA%90%E5%BC%80%E5%85%B3/%E5%BC%80%E5%85%B3%E7%94%B5%E6%BA%90%E8%AE%BE%E8%AE%A1/m-p/695987
Show LessHello, refering to EVAL-PFC5KIKWWR5SYS I already reduced the output voltage down to load my capacitor bank rated 350Vdc. Now I would like to limit the power to 3kW in environment where 16A magneto Thermal protection is mount. Where I can act? thanks in advance Stefano
Show LessI am a student. Could you please recommend a suitable driver for the IRG4BC40KD N-Channel IGBT Transistor 42A 600V TO-220 model transistor? Would this driver be suitable for my needs?
https://pdf.direnc.net/upload/irg4bc40kd-datasheet.pdf
https://dosya.motorobit.com/pdf/A316J.pdf
Hello! We performed ltspice double pulse test simulations on Infineon's three IGBT chips (models IKW75N65EL5_L1, IKZA75N65RH5_L1, and IKZA75N65RH5_L1, respectively). We found that during the IGBT switching process, the waveform in Figure 2 shows that the gate voltage suddenly drops after the Miller platform. The gate voltage waveform of some chips even reached negative pressure during this drop. At the same time, the experimental and simulation waveforms can also correspond to the simulation waveforms. I don't know if this kind of waveform is normal, I'd like you to explain it.
ltspice simulation waveform
ltspice simulation
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/%E5%8F%8C%E8%84%89%E5%86%B2%E5%AE%9E%E9%AA%8C%E4%B8%8E%E4%BB%BF%E7%9C%9F%E6%97%B6%E5%8F%91%E7%8E%B0%E9%97%A8%E6%9E%81%E7%94%B5%E5%8E%8B%E5%87%BA%E7%8E%B0%E7%9F%AD%E6%9A%82%E4%B8%8B%E9%99%8D%E7%9A%84%E9%97%AE%E9%A2%98-%E4%B8%8D%E7%9F%A5%E9%81%93%E6%98%AF%E5%90%A6%E6%AD%A3%E5%B8%B8/td-p/684353
Show LessHello, what are the pins on top of the IGBT module in figure 1 below? Is there any correspondence between these terminals and the endpoints in figure 2?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IGBT%E6%A8%A1%E5%9D%97%E7%AB%AF%E5%AD%90/td-p/687990
Show LessWhat is an alternative chip or solution to use IR25750LTRPBF (discontinued) to detect conduction voltage drop
The bus voltage is 400V, and the withstand voltage is about 600
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IGBT-MOSFET%E7%89%B9%E6%80%A7%E7%A0%94%E7%A9%B6/td-p/684372
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/IBGT%E6%A8%A1%E5%9D%97/td-p/687996
Show Less