Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

IGBT Forum Discussions

Translation_Bot
IGBT
When aging tests are performed on igbt devices, it can be concluded that the aging devices will have changes in Vce, Vth, and a host of other paramete... Show More
Translation_Bot
IGBT
ASC/FW
solved msg Solved
Hello Infineon: Hello, I am an electric vehicle practitioner, I have a question about the logic of ASC, is there any difference between the upper and ... Show More
infineon_sic
IGBT

in the datasheet,Why the Isolation test voltage for 1200V IGBT Module is 2.5kV,how to define ?

ricardosf
IGBT
In our technical assistance department we need to desolder and remove defective IGBT MODULES like FS3L30R07W2H3F_B11 from the PCB to replace by new IG... Show More
Translation_Bot
IGBT
IGBT Modules
solved msg Solved
Hello engineers: I would like to know more about this IGBT module FF100R12KS4 and have some questions, does this model make a Kelvin emitter? If so, a... Show More
1003653144
IGBT
FZ300R12KE3G
solved msg Solved

工程师您好:

           关于FZ300R12KE3G此款IGBT型号,我想询问一下,5号管脚是否为开尔文发射极,2号引脚是否为主发射极?

 

CiroCampos85
IGBT
Hi, looking for a similar documentation from Infineon regarding the topic "Humidity and Condensation on Power Electronics".Can someone help me by send... Show More
乱世煮酒论天下
IGBT
IGBT应用在变频器中,在开通过程中,在设计驱动电路中做出了一种保护,就是针对CE结压降的一种保护,就是使导通的IGBT的CE压降尽可能处在一个比较小的范围,请问这个完全饱和的导通压降一般是多少伏? IGBT的CE可以看做是三极管,为什么会在完全导通的状态存在导通压降? 在IGBT开通的时候,CE压... Show More
LouieLiu
IGBT
大家好,IGBT使用的开通电压是15V,关断电压是0V,IGBT门极信号关断后产生一个3-6V的电压尖峰,超过IGBT的阈值电压,可能导致误开通。请教一下该电压尖峰的产生机理以及如何解决该现象。谢谢!#FS75R12KT4_B15 Show More
乱世煮酒论天下
IGBT
在IGBT短路时,示波器测量IGBT栅极驱动的电压,发现栅极电压会在极短的时间内产生振荡,最后会回到负关断电压。请问这是什么原因? 相应的,在IGBT短路时,IGBT的CE电压在驱动开通时,电压是低电平,当发生短路时,CE电压会迅速上升然后下降直到母线电压的一半,在CE电压上升的过程中会在最大值的尖... Show More
Forum Information

IGBT

Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.