Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

IGBT Forum Discussions

Sort by:
mountee
IGBT
1、采用两片IR2103驱动一个H桥,开关管采用SGL160N60UFDTU,负载为一个线圈,电感约为40mH,电阻2.4Ω,线圈正向通电时间为44ms,反向通电时间为14ms,门极开通电阻为22Ω,关断电阻为0Ω,门极对发射极有16V稳压管,如图所示,线圈正反向通电时间间隔20秒以上   2、操... Show More
Translation_Bot
IGBT
The minimum driving peak current value in the specification is 2A, and the typical values are 4A and 3.5A respectively. When driving the CIB module, t... Show More
Translation_Bot
IGBT
Lithium battery protection board project, high-side NMOS tube controls charging/discharging circuit. Now, a gate driver chip, IRS25752LTRPBF, has been... Show More
Translation_Bot
IGBT
Please explain in detail the basic test circuit and test process of the IGBT module for parameters such as reverse recovery peak current, recovery cha... Show More
fallma
IGBT
I wish to lower the output voltage of the EVAL-PFC5KIKWWR5SYS from 400V to 300V. Does someone know how to do that ?  thanks  Show More
YuTa_4942221
IGBT
PressFtiに関して1点確認させてください。 下記ANに記載している補助治具に関してですが、こちらはInfineon様が設計しているとANに記載がございますが、Infineon様からご提供は可能という事でしょうか? AN P6抜粋   実際にPressIn、PressOutする治具はお客様の方... Show More
Translation_Bot
IGBT
Internal block diagram according to the IR2103 manual Undervoltage lockout only involves VCC. If the high side uses bootstrap power supply, does it a... Show More
EM4user
IGBT
麻烦工程师介绍一下两者的不同,并推荐英飞凌相关产品和学习资料,非常感谢! 原帖链接如下: https://www.zhihu.com/question/604700277 Show More
JGPark1970
IGBT
Hi,  hi?I am trying to operate an Axial flux machine using Hybridkit Drive sense.While running the position sensor wizard for the first task, I discov... Show More
aaa4
IGBT

我在做igbt负载自适应驱动的相关的科研,我希望从igbt关断时的米勒平台推算出此刻的负载电流,如果能实现这一点,且准确性有保证,那么在igbt下一次开通时,实际的负载电流会与上一次关断时的负载电流变化很多吗,也就是负载电流会在igbt开通关断的时间间隔上发生很大的瞬变吗

Forum Information

IGBT

Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.