IM818LCC无法启动

公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
hello110300509
Level 1
Level 1
First reply posted First question asked Welcome!

您好,我购买了IM818LCC,对他施加了100——400V的母线电压,并提供了开关信号(5V),然而,模块始终无法实现开关,请问这是什么问题?原理图见附件,请注意:G1_12V_XX等网络提供的是14.8V电源,经过测试是正常的。谢谢,急切等待指导。

0 点赞
1 解答
Rachel_G
Moderator
Moderator
Moderator
50 likes received 250 solutions authored 250 replies posted

Hello,

如果基于调试目的,只考虑IPM模块,不考虑其他辅助电源/MCU等条件的限制,该模块是可以在48V电压工作的。

谢谢!

Rachel

在原帖中查看解决方案

0 点赞
6 回复数
Rachel_G
Moderator
Moderator
Moderator
50 likes received 250 solutions authored 250 replies posted

您好,

在您上传的原理中,只包含功率部分,请问您的控制输入PWM信号是如何实现的?建议检查该模块的输入PWM信号是否正确,如果输入开关信号不正常,该模块也是无法正常工作的。另外针对该模块我们有相对应的demo板和控制板,您可以参考demo 板设计进行调整优化您的板子。链接如下:

https://www.infineon.com/cms/en/product/evaluation-boards/eval-m1-im818-a/

https://www.infineon.com/cms/en/product/evaluation-boards/eval-m1-101t/

谢谢!

Rachel

 

0 点赞
lock attach
Attachments are accessible only for community members.

十分感谢您的回复,附件是提供的开关信号,开关信号电平为5V,由ISO7721输出;我看参考设计的RFE、ITRIP和我的原理图差异较大,您认为是否有问题;此外,我想了解下这个模块能否在母线电压为36V,48V下工作,谢谢!

0 点赞
喜马拉雅之雪
Employee

R12值,有点太大了。建议测下各管脚电压,以保证供电或状态正常。

另外;建议按演示版修改原理和PCB图。如果PCB布局不当,仍然是无法工作的。

至于母线电压,IPM本身并无探测。但;MCU通常会以此作为控制参量,并设置有上下限。

0 点赞
Rachel_G
Moderator
Moderator
Moderator
50 likes received 250 solutions authored 250 replies posted

您好,

对于母线电压,请参考数据手册中的正常工作推荐值,最小值为350V。

Rachel_Gao_0-1689299398965.png

谢谢!

Rachel

0 点赞
hello110300509
Level 1
Level 1
First reply posted First question asked Welcome!

谢谢,因为现在调试的时候,希望上个小点的电压,比如48V,这样比较安全。我想知道48V情况下,IM818是否能正常开关,谢谢!

0 点赞
Rachel_G
Moderator
Moderator
Moderator
50 likes received 250 solutions authored 250 replies posted

Hello,

如果基于调试目的,只考虑IPM模块,不考虑其他辅助电源/MCU等条件的限制,该模块是可以在48V电压工作的。

谢谢!

Rachel

0 点赞