Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

IGBT Forum Discussions

somedisatance
Level 1
Level 1
First reply posted First question asked Welcome!

HI:

I want to design a circuit for my product

Input voltage required:≤150~200V

Output voltage:36V

output power:≥100W

Service temperature:150℃

Are there any recommended designs that can be used?

Thanks

0 Likes
1 Solution
tengD
Moderator
Moderator
Moderator
50 sign-ins 50 solutions authored 5 likes given

@somedisatance ,

Service temperature:150℃  -->what is the service temperature?

My understanding is ambient tempertautre, If yes, then since most of the driver ICs maximum operating temperature is upto 150℃, when operating there's some loss on the IC, so no possible to work with 150℃ ambient temerature.

View solution in original post

0 Likes
3 Replies
tengD
Moderator
Moderator
Moderator
50 sign-ins 50 solutions authored 5 likes given

@somedisatance ,

Service temperature:150℃  -->what is the service temperature?

My understanding is ambient tempertautre, If yes, then since most of the driver ICs maximum operating temperature is upto 150℃, when operating there's some loss on the IC, so no possible to work with 150℃ ambient temerature.

0 Likes

You understand correctly, but this is only one indicator. Generally, devices with a nominal temperature of 150 ℃ can be used. Is there a recommended circuit or IC?

0 Likes
tengD
Moderator
Moderator
Moderator
50 sign-ins 50 solutions authored 5 likes given

@somedisatance ,

I have checked in our product lines, no suitable recommendations as the 150 ℃ is required.

 

0 Likes