Announcements

Curious on how you can apply IGBT to Smart Home Appliances? Register for the ASEAN Smart Home Appliance Webinar here to find out how.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

IGBT Forum Discussions

Fränce
Moderator
Moderator 5 sign-ins 5 replies posted 10 questions asked
Moderator
Dear community,

what is the recommended frequency range for operating IGBT T7?

Thanks,
Fränce
0 Likes
1 Solution
Giuseppe_De_Fal
Moderator
Moderator 10 solutions authored 10 replies posted 10 sign-ins
Moderator
Hi Fränce,
T7 technology is specifically designed for industrial motor drive applications and solar energy systems with a switching frequency range between 5kHz and 30kHz.

You can find further information on this page: https://www.infineon.com/cms/en/product/power/igbt/trenchstop-igbt7/.

Regards,
Giuseppe

View solution in original post

0 Likes
4 Replies
Giuseppe_De_Fal
Moderator
Moderator 10 solutions authored 10 replies posted 10 sign-ins
Moderator
Hi Fränce,
T7 technology is specifically designed for industrial motor drive applications and solar energy systems with a switching frequency range between 5kHz and 30kHz.

You can find further information on this page: https://www.infineon.com/cms/en/product/power/igbt/trenchstop-igbt7/.

Regards,
Giuseppe
0 Likes
User17687
Level 1
5 questions asked First question asked First reply posted
Level 1
Good morning,

which devices is IGBT T7 targeting to replace? And what are the improvements compared to the predecessors?

Thanks,
Walter
0 Likes
Giuseppe_De_Fal
Moderator
Moderator 10 solutions authored 10 replies posted 10 sign-ins
Moderator
Hello Walter,
sorry for the late reply.

The T7 IGBT and diode technology has been released as a flexible series to replace existing Infineon’s short-circuit rated product families, such as TRENCHSTOP™, TRENCHSTOP™ Performance, and HighSpeed 3.
It can also be used as an alternative to the non-short-circuit rated TRENCHSTOP™5 technologies.

IGBT7 T7, in a comparison with predecessor generations, increase the system power capability by up to 25%, while maintaining a similar temperature of the devices. At same system power, IGBT7 T7 can be driven with up to 15% lower junction temperature compared to the aforementioned existing technologies.
In addition, the IGBT7 T7 blocking voltage has been increased by 50V in comparison with previous generations and now it is rated at 700V.

For more information, you can refer to the following material:
IGBT7 T7 Product presentation:
https://www.infineon.com/dgdlac/Infineon-Sales_Call-650V_TRENCHSTOP_IGBT7_T7-ProductPresentation-v01...
IGBT7 T7 Application note:
https://www.infineon.com/dgdl/Infineon-AN2020-15_Introduction_to_Discrete_650V_TRENCHSTOP_IGBT7_T7-A....

Best Regards,
Giuseppe
0 Likes
User17675
Level 1
5 questions asked First question asked First reply posted
Level 1
Is there any plan for a portfolio extension e.g. AirCon PFC application?
0 Likes