Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.
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
Greetings! Regarding the use of the Infineon TLE8366 (i.e. the attached pdf), please ask

1. What kind of power supply is connected to pins 7 and 8 in Figure 1 of the attached word document?

2. Is the UNDER_VOL_DETECTION module in Figure 2 of the attached word document also this type of power supply?

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/IGBT/DCDC%E9%99%8D%E5%8E%8B%E5%99%A8/td-p/693134

0 Likes
1 Solution
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello,

1. The power supply in Figure 1 is a three day bus for the automotive KL30 15 31. However, this is not a hard and fast requirement and for other applications it can be designed according to the requirements of the application system itself as long as the voltage is within SPEC.

2. The module in Figure 2 is not a power supply, but a low voltage detection module designed to pull down the EN under under undervoltage conditions, and there are many ways to realize this, which can be designed according to the specific application requirements.

Dipping,

Xiangrui

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%BA%90%E7%AE%A1%E7%90%86%E8%8A%AF%E7%89%87/DCDC%E9%99%8D%E5%8E%8B%E5%99%A8/m-p/695986

View solution in original post

0 Likes
5 Replies
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello.

Please find below answers

1. What kind of power supply is connected to pin 7 and pin 8 in Figure 1 of the attached word document?

== > They are PI filters used for noise filtering at pin No.8

Pin 7 has filter cap .

2. Is the UNDER_VOL_DETECTION module in Figure 2 of the attached word document also a type of power supply?

== > Please share complete circuit so that we can help ,But initially it looks like Power supply which used power enable pin and that have Under voltage_ protection modeled internally. Protection modeled internally.

Check out the answers below

1. Which power supply is connected to pins 7 and 8 in Figure 1 of the attached word document?

Pin 7 has a filter cap.

2. Is the undervoltage protection module in Figure 2 of the attached word document also a type of power supply?

Thanks

Mohan N

 

 

 

 

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%BA%90%E7%AE%A1%E7%90%86%E8%8A%AF%E7%89%87/DCDC%E9%99%8D%E5%8E%8B%E5%99%A8/m-p/694199

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello, Figure 2 of the attached word document is Figure 33 of the following document. it is reported that this driver board has been discontinued by your company, and I would like to know more detailed information about this driver board for the purpose of learning. I would like to know more details about this driver board for learning purpose. What module is UNDER_VOL_DETECTION in Figure 33 of the following document ? I hope you do not hesitate to give me advice, and wish me a happy new year!

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%BA%90%E7%AE%A1%E7%90%86%E8%8A%AF%E7%89%87/DCDC%E9%99%8D%E5%8E%8B%E5%99%A8/m-p/694213

0 Likes
lock attach
Attachments are accessible only for community members.
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello, the original question in the word document Figure 2 for the current reply attached pdf file Figure 33

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%BA%90%E7%AE%A1%E7%90%86%E8%8A%AF%E7%89%87/DCDC%E9%99%8D%E5%8E%8B%E5%99%A8/m-p/695128

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello leer,

这里设计的是一个欠压检测功能,如果输入电压欠压输出低电平,TLE8366EV无法使能,系统进入关闭状态。

这里并未被配欠压保护电路,因此不具有欠压保护功能。

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/Re-DCDC%E9%99%8D%E5%8E%8B%E5%99%A8/m-p/696043

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello,

1. The power supply in Figure 1 is a three day bus for the automotive KL30 15 31. However, this is not a hard and fast requirement and for other applications it can be designed according to the requirements of the application system itself as long as the voltage is within SPEC.

2. The module in Figure 2 is not a power supply, but a low voltage detection module designed to pull down the EN under under undervoltage conditions, and there are many ways to realize this, which can be designed according to the specific application requirements.

Dipping,

Xiangrui

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%BA%90%E7%AE%A1%E7%90%86%E8%8A%AF%E7%89%87/DCDC%E9%99%8D%E5%8E%8B%E5%99%A8/m-p/695986

0 Likes