cancel
Showing results for 
Search instead for 
Did you mean: 

IGBT Modules

User17756
New Contributor
Hi all,

can someone explain the difference between the EconoPack+ B and D series?
For example, 450A 1200V device is available in both versions.


Thanks!
0 Likes
1 Reply
AlexG
Moderator
Moderator
Hi JoFoe,

First of all pin and power terminal positions of EconoPACK™+ D-series as well as module dimensions are identical to EconoPACK™+ B-series.
D-series modules has following improvements:
- lower internal inductivity;
- ultrasonic welded power terminals;
- pressFIT control terminals;
- injection molded power and control terminals;
- improved TC curve.

Infineon recommends to use EconoPACK™+ D-series for the new designs.
You can find more information here.

BR
0 Likes