cancel
Showing results for 
Search instead for 
Did you mean: 

IGBT Modules

User22320
New Contributor
Select models: FF300R12ME4 and FF300R17ME4. Intend to use the IGBT internal NTC resistor as the overheat protection sampling. What temperature is appropriate for the overheat protection setting?


选用型号:ff300r12me4和ff300r17me4. 打算使用igbt内部的ntc电阻作为过热保 护 采样,过热保护点设置到多少温度合 适 ?
0 Likes
1 Reply
AlexG
New Contributor
Dear Walt,

The delta between the temperature of the NTC and the Tvj differs under different cooling conditions.
We cannot give a universal advice that works for all operating conditions of the modules.
To accurately determine this delta under certain operation conditions, it is best to measure the temperatures inside a module with an IR camera.
To do this you will need black painted modules with no gel inside.
Other option is the modules with thermocouples glued to the chips inside the module.

You can order both options through your sales channel.

Some further details about the use of NTC you can find here.

BR
AlexG
0 Likes
Top labels