Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MS_19060803
Level 6
Level 6
Distributor - TED (Japan)
25 likes received 25 solutions authored 10 likes given

Hi all,

The Ic(sc) of IKD15N60RF is described as 112A in the data sheet.
Is there a recommended current value to protect the short circuit?
As a condition, they keep the short circuit time.

Best regards,
MS

0 Likes
1 Solution

Hello,
Yes, it is. But as it is an estimated value, not verified, better to analyze the value from the graph as these are tested short circuit ratings against some fixed conditions.

Regards,
Anshika

Regards,
Anshika

View solution in original post

0 Likes
3 Replies
Anshika_G
Moderator
Moderator
Moderator
First question asked 50 likes received 250 replies posted

Hello,
Thank you for posting on Infineon Community.

The short circuit rating is a measure of the energy that the IGBT can withstand under a short circuit condition.  In this condition, the IGBT is forced on, with a high voltage applied across the collector-emitter terminals.  This causes a very high current to flow and very high power levels to be dissipated by the device.

The short circuit rating is tested by applying a fixed voltage across the collector-to-emitter terminals and then biasing the gate on.  This is tested while the IGBT is mounted on a heat sink and stabilized at a high temperature.  In IKD15N60RF, i.e. ,a 600 V IGBT, we typically apply 300 to 400 V from the collector-to-emitter terminals and then bias the gate at 15 V.  The short circuit current rating  on our datasheets are measured on these test conditions. The below figure shows , t(sc) and Ic(sc) behavior can be mapped as the function of the gate voltage VGE(refer datasheet, page 11).

G_Anshika_0-1652679234517.png

One can measure Ic(sc) value by measuring slope of the curve for a given VGE value.
If you still need a recommenced value for the current, with state-of-the-art IGBTs, it is usually rated at 3~6 times nominal current to keep a high level of reliability as well as lifetime. 

Note - It is highly recommended to go with datasheet parameters to make best use of product and it's safety.

Thanks and Regards,
Anshika

0 Likes
MS_19060803
Level 6
Level 6
Distributor - TED (Japan)
25 likes received 25 solutions authored 10 likes given

Hi,

Does IKD15N60RF correspond to the following explanation?
If you still need a recommenced value for the current, with state-of-the-art IGBTs,
it is usually rated at 3~6 times nominal current to keep a high level of reliability as well as lifetime.

Best regards,
MS

0 Likes

Hello,
Yes, it is. But as it is an estimated value, not verified, better to analyze the value from the graph as these are tested short circuit ratings against some fixed conditions.

Regards,
Anshika

Regards,
Anshika

0 Likes