Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Hyper RAM Forum Discussions

Sort by:
lukasfrank
Hyper RAM
Hi Dear Authorized,   I am trying to use HyperRAM over FlexSPI Interface and some errors occured during test on my custom board which suited by NXP IM... Show More
openchip
Hyper RAM
Hi we see memory test failures when running memtest in an eternal loop, it happens about once a day, and once it was running a week without failures. ... Show More
MAO
Hyper RAM
When I set up HyperBUS, it writes an indeterminate value (this is usually the case in the first generation as well).When I write after this, I cannot ... Show More
JeanL
Hyper RAM
Hello,On our board we have one HyperRAM (S27KS064 1 DP B HB 02) and one HyperFlash (S26KS512S DP B HM 02).These memories are connected to a FPGA throu... Show More
Braycarl
Hyper RAM
In Hyper-V what happens when I "delete saved state" of one Remote PC; Would I lose the data in that Remote PC? Because I have tried to increase the RA... Show More
Berkj
Hyper RAM
Hello everyone, I asked the same question under HyperFlash board; however, this applies to the HyperRAM too since they follow the HyperBus timing spec... Show More
GoKo_4683011
Hyper RAM
Hello, We are using the STM32L4R5 (Nucleo-144, L4R5ZI-P) to implement HyperRAM memory (S27KL0642) under hyperbus protocol. There is a problem between ... Show More
Stark38
Hyper RAM
Hi, I'm trying to implement Hyperbus protocol for Hyper RAM on a NUCLEOL4R5ZI-P without success. Is some exemple on STM32L4R are available?   Kind reg... Show More
pf_arc
Hyper RAM
We are using a Cypress/Infineon HyperRAM, part number S70KS1281DPBHV020, driven by the Cypress/Infineon Hyperbus Controller on a Xilinx FPGA (xc7k160t... Show More
GirijaC
Hyper RAM
The demo showcases the HyperRAM in Industrial or consumer HMI application as an expansion Memory in Display Applications. This demo demonstrates the H... Show More
Forum Information

Hyper RAM

HyperRAM™ memory Forum discusses self-refresh DRAM operating on the 12-pin HyperBus interface. With a read throughput up to 333 MB/s, the HyperRAM for SoCs with limited on-board RAM providing external scratch-pad memory for fast read and write operations.