Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

BeCr_3107286
Level 1
Level 1

Can the hyperbus spec tolerate a 1ns delay in clock? My MCU only has a single ended clock output at 1.8v - I could use a pair of fast XOR gates to convert to psuedo differential. Has this been tried, is there a recommended way to do this? Will be running <100MHz for low power application.

Thanks.

1 Solution

Thanks for the information.

The CK/CK# delay relative to DQ and RWDS impacts to the Input Hold timing (tIH) spec in the HyperRAM. The minimum requirement for tIH in the 1.8V HyperRAM is 0.6ns (https://www.cypress.com/file/183506/download ). In the STM datasheet (https://www.st.com/resource/en/datasheet/stm32l4s5qi.pdf ), the data output hold time, thr/thf(OUT) is specified for some different conditions. If 1ns delay is generated by the XOR, the output hold time should satisfy thr/thf(OUT) - 1ns > 0.6ns. I'm not sure if it is feasible, but it sounds difficult...

Thanks,

Takahiro

View solution in original post

0 Likes
3 Replies
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi Ben,

We would like to clarify,

1) What MCU is being used ?

2) What flash or HyperRAM part you are using ?

3) What is this delay to ? The CK# can delay 1ns to the CK, or CK/CK# can delay to the DQ input ?

If you are using Hyperflash, the Semper S26HS family do not need CK# so using that could also be a solution.

Thanks,
Pradipta.

0 Likes

MCU: ST Micro STM32L4S5QII @ 1.8v - hyperbus port - single ended clock only

Any Cypress HyperRAM chip ok, prefer 8MB, 105C

Will insert a logic delay of 1ns converting single ended clock to differential clock relative to all other signals.

Propose to use two very fast 1.8v XOR gates on clock (in parallel) to create a pair of complementary clock signals.

TI Gate: SN74AUC2G86YZPR

Is there a better way? Would this work? It would close up eye diagram a bit...

0 Likes

Thanks for the information.

The CK/CK# delay relative to DQ and RWDS impacts to the Input Hold timing (tIH) spec in the HyperRAM. The minimum requirement for tIH in the 1.8V HyperRAM is 0.6ns (https://www.cypress.com/file/183506/download ). In the STM datasheet (https://www.st.com/resource/en/datasheet/stm32l4s5qi.pdf ), the data output hold time, thr/thf(OUT) is specified for some different conditions. If 1ns delay is generated by the XOR, the output hold time should satisfy thr/thf(OUT) - 1ns > 0.6ns. I'm not sure if it is feasible, but it sounds difficult...

Thanks,

Takahiro

0 Likes