S70KS1281DPBHI023 - Thermal Resistance and Tj

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Sade_4357781
Level 1
Level 1

I am looking for Thermal Resistance and Temperature Junciton Max...

Thanks!

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

The Theta Ja is 55 C/W and the Psi Jt is 0.14 C/W

Please refer to the following app note for more information on the Psi Jt parameter.

https://www.cypress.com/file/210756/download

The Maximum Junction Temperature that the device can bear is 125 C. Please note that you will need to maintain the Tj of the device less than this value or it can lead to some permanent damage to the device.

Thanks,

Pradipta.

View solution in original post

0 Likes
1 Reply
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

The Theta Ja is 55 C/W and the Psi Jt is 0.14 C/W

Please refer to the following app note for more information on the Psi Jt parameter.

https://www.cypress.com/file/210756/download

The Maximum Junction Temperature that the device can bear is 125 C. Please note that you will need to maintain the Tj of the device less than this value or it can lead to some permanent damage to the device.

Thanks,

Pradipta.

0 Likes