Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Hyper RAM Forum Discussions

Stark38
Level 1
10 sign-ins 5 replies posted 5 sign-ins
Level 1

Hi,

I'm trying to implement Hyperbus protocol for Hyper RAM on a NUCLEOL4R5ZI-P without success. Is some exemple on STM32L4R are available?

 

Kind regards

0 Likes
3 Replies
PradiptaB_11
Moderator
Moderator 500 replies posted 250 solutions authored 250 replies posted
Moderator

Hi,

Currently we do not have any code examples for the Hyberbus protocol with us. If possible we can work on the code you have till now and try to implement it for the Nulceo board. If it is ok can you share the code with us.

Thanks,

Pradipta.

0 Likes
Stark38
Level 1
10 sign-ins 5 replies posted 5 sign-ins
Level 1

HI,

 

Yes no problem!

void ospi_config(void)
{
	//OCTOSPI IO Manager clock enable
	  RCC->AHB3ENR |= RCC_AHB3ENR_OSPI1EN;
	//OCTOSPI1 clock enable
	  RCC->AHB2ENR |= RCC_AHB2ENR_OSPIMEN;
  //CR REGISTER
	//OCTOSPI1 enable
	  OCTOSPI1->CR |= OCTOSPI_CR_EN;
	 //INDIRECT write
	  OCTOSPI1->CR |= (0 << OCTOSPI_CR_FMODE_Pos);
	  OCTOSPI1->CR |= (5 << OCTOSPI_CR_FTHRES_Pos);
  //DCR1 REGISTER
	  //REGISTER SPACE
	  OCTOSPI1->DCR1 |= (5 << OCTOSPI_DCR1_MTYP_Pos);
	  //DEVICE SIZE = 26
	  OCTOSPI1->DCR1 |= (0x1A << OCTOSPI_DCR1_DEVSIZE_Pos);
	  //CHIPSELECT HIGH TIME = 1cycle
	  OCTOSPI1->DCR1 |= (0 << OCTOSPI_DCR1_CSHT_Pos);
	  //DELAYBLOCK NOT BYPASSED
	  OCTOSPI1->DCR1 |= (0 << OCTOSPI_DCR1_DLYBYP_Pos );
	  //FREERUNING CLOCK DISABLED
	  OCTOSPI1->DCR1 |= (0 << OCTOSPI_DCR1_FRCK_Pos);
	  //CLOCK MODE = LOW
	  OCTOSPI1->DCR1 |= (0 << OCTOSPI_DCR1_CKMODE_Pos);
  //DCR2 REGISTER
	  //CLOCK PRESCALER = 3
	  OCTOSPI1->DCR2 |= (2 << OCTOSPI_DCR2_PRESCALER_Pos);
  /****** CCR REGISTER ******/
	  //INSTRUCTION SENT ON EVERY TRANSACTION
	  OCTOSPI1->CCR |=  (0 << OCTOSPI_CCR_SIOO_Pos);
	  //DQS Enable
	  OCTOSPI1->CCR |= OCTOSPI_CCR_DQSE;
	  // DDTR enable
	  OCTOSPI1->CCR |= OCTOSPI_CCR_DDTR;
	  //DATA on a single line
	  OCTOSPI1->CCR |= OCTOSPI_CCR_DMODE_0;
	  //16-bytes Address size
	  OCTOSPI1->CCR |= OCTOSPI_CCR_ADSIZE_0;
	  //Address DTR enable
	  OCTOSPI1->CCR |= OCTOSPI_CCR_ADDTR;
	  //Address on a single line
	  OCTOSPI1->CCR |= OCTOSPI_CCR_ADMODE_0;
	  //DHQC enable
  /***** TCR REGISTER *****/
	  OCTOSPI1->TCR |= OCTOSPI_TCR_DHQC;
	  //5 dummy cycles
	  OCTOSPI1->TCR |= (5 << 0);
  /***** WTCR REGISTER *****/
	  //5 dummy cycles in write operation
	  OCTOSPI1->WTCR |= (5 << 0);
  /***** WCCR REGISTER *****/
	  OCTOSPI1->WCCR |= OCTOSPI_WCCR_DQSE;
	  //DSQ Enable
	  OCTOSPI1->WCCR |= (OCTOSPI_WCCR_DQSE);
	  //DDTR Enable
	  OCTOSPI1->WCCR |= (OCTOSPI_WCCR_DDTR);
	  //Data on single line
	  OCTOSPI1->WCCR |= (OCTOSPI_WCCR_DMODE_2) ;
	  OCTOSPI1->WCCR |= (OCTOSPI_WCCR_ADSIZE_0);
	  OCTOSPI1->WCCR |= (OCTOSPI_WCCR_ADDTR);
	  OCTOSPI1->WCCR |= (OCTOSPI_WCCR_ADMODE_0);
  /***** HCLR ******/
	  // Trwr = 4 clk
	  OCTOSPI1->HLCR |= (4 << OCTOSPI_HLCR_TRWR_Pos);
	  //Tacc = 4 clk
	  OCTOSPI1->HLCR |= (4 << OCTOSPI_HLCR_TACC_Pos);
	  //Variable latency
	  OCTOSPI1->HLCR |= (0 << OCTOSPI_HLCR_LM_Pos);
}
void ospi1_write_reg(uint32_t tdata, uint32_t add)
{
	 //INDIRECT write
	  OCTOSPI1->CR |= (0 << OCTOSPI_CR_FMODE_Pos);
	  //REGISTER SPACE + HYPERBUS
	  OCTOSPI1->DCR1 |= (5 << OCTOSPI_DCR1_MTYP_Pos);
	  OCTOSPI1->AR = add;
	  OCTOSPI1->DR |= tdata;
	  OCTOSPI1->DLR = 4;
	  while( ((OCTOSPI1->SR & OCTOSPI_SR_BUSY_Msk) >> OCTOSPI_SR_BUSY_Pos == 1))
	  {
		  HAL_Delay(1);
	  }
	  if(((OCTOSPI1->SR & OCTOSPI_SR_TCF_Msk ) >> OCTOSPI_SR_TCF_Pos) == 1 )
	  {
		  OCTOSPI1->FCR |= OCTOSPI_FCR_CTCF;
	  }
}

void ospi1_read_reg(uint32_t add)
{

	  OCTOSPI1->AR = 0x00010000;
		//INDIRECT Read MODE
		  OCTOSPI1->CR |= (1 << OCTOSPI_CR_FMODE_Pos);

		  //REGISTER SPACE
		  OCTOSPI1->CCR |=  (0 << OCTOSPI_CCR_SIOO_Pos);
		  //DQS Enable
		  OCTOSPI1->CCR |= OCTOSPI_CCR_DQSE;
		  // DDTR enable
		  OCTOSPI1->CCR |= OCTOSPI_CCR_DDTR;
		  //DATA on a single line
		  OCTOSPI1->CCR |= (0 << OCTOSPI_CCR_DMODE_Pos);
		//  OCTOSPI1->CCR |= OCTOSPI_CCR_ABMODE_0;
		  //16-bytes Address size
		  OCTOSPI1->CCR |= OCTOSPI_CCR_ADSIZE_0;
		  //Address DTR enable
		  OCTOSPI1->CCR |= OCTOSPI_CCR_ADDTR;
		  //Address on a single line
		  OCTOSPI1->CCR |= OCTOSPI_CCR_ADMODE_0;

	  while( ((OCTOSPI1->SR & OCTOSPI_SR_BUSY_Msk) >> OCTOSPI_SR_BUSY_Pos == 1))
	  {

	  }
	  if(((OCTOSPI1->SR & OCTOSPI_SR_TCF_Msk ) >> OCTOSPI_SR_TCF_Pos) == 1 )
	  {
		  OCTOSPI1->FCR |= OCTOSPI_FCR_CTCF;
	  }
	  pData = OCTOSPI1->DR;
}

 

Thank you!

0 Likes
Stark38
Level 1
10 sign-ins 5 replies posted 5 sign-ins
Level 1

Can we have a hope to solve this issue with your help?

Thanks!

0 Likes