Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
user_4064026
Level 1
Level 1

Hello,

Can we feed Hyperram's CK and CK#  diffirential clock buses with SSTL18I io standard? I read that Hyperram's inputs and outputs are LV-CMOS compatible on datasheet.

Do we have to use LVCMOS18 io standart for clock buses with 1.8V devices?

Best Regards,

Emre

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

The Hyper RAM I/Os are compatible with LV-CMOS standards. We can suggest you to use LVCMOS for best fit option.

Theoretically SSTL standard calls for an external termination. This external termination can only affect the voltage swing of the signal. The other important parameters like VIL, VIH, VOL, VOH are very similar for the two standards. If the external termination affects the voltage swing by a small fraction you can also use SSTL signalling. 

I encourage you to use the IBIS model for hyper Ram and try this out.

https://community.cypress.com/external-link.jspa?url=http%3A%2F%2Fwww.cypress.com%2Fproducts%2Fhyper...

Thanks,

Pradipta.

View solution in original post

0 Likes
1 Reply
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

The Hyper RAM I/Os are compatible with LV-CMOS standards. We can suggest you to use LVCMOS for best fit option.

Theoretically SSTL standard calls for an external termination. This external termination can only affect the voltage swing of the signal. The other important parameters like VIL, VIH, VOL, VOH are very similar for the two standards. If the external termination affects the voltage swing by a small fraction you can also use SSTL signalling. 

I encourage you to use the IBIS model for hyper Ram and try this out.

https://community.cypress.com/external-link.jspa?url=http%3A%2F%2Fwww.cypress.com%2Fproducts%2Fhyper...

Thanks,

Pradipta.

0 Likes