- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello everyone,
I asked the same question under HyperFlash board; however, this applies to the HyperRAM too since they follow the HyperBus timing specification all together.
Here is the link to the question: (Please review it, I'm not pasting it here to not to duplicate)
For the CLK, DQ and RWDS timings, it seems like the datasheet values are valid only up to ~65 MHz, although it is specified up to 133 MHz. Delay values and the valid areas of given signals doesn't add up and there seems to be a mismatch.
Has anyone ever tried to design the interface themselves or debugged the interface above ~65 MHz (CLK)? I'd like to see the DQs and RWDS signals (measured) above these clock frequencies.
Hopefully, @BushraH_91 , @TakahiroK_16 or other employees can answer. In the meantime, please feel free to comment if you're experienced on the topic.
Thank you.
- Labels:
-
Memory Hyper RAM