Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Hyper RAM Forum Discussions

AlUz_4821276
Level 1
Level 1
First like given

How many mixed of HyperRAM / HyperFlash can exist on the same bus? What are the limitations and critical points?

e.g.

2x HyperRAM  + 1 x HyperFlash

1x HyperRAM  + 2 x HyperFlash

Thx.

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

There are no limitations from the device side. every chip will have a separate CS pin which can be used to select any required device. The controller drive strength will be the limiting factor for this selection and what are the design requirements. If the controller can support more fan out you can have more chips sharing the address and data lines. Both the configuration that you have mentioned as an example, we have seen them implemented. You can also check our layout guidelines for more information.

Thanks,

Pradipta.

View solution in original post

2 Replies
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

There are no limitations from the device side. every chip will have a separate CS pin which can be used to select any required device. The controller drive strength will be the limiting factor for this selection and what are the design requirements. If the controller can support more fan out you can have more chips sharing the address and data lines. Both the configuration that you have mentioned as an example, we have seen them implemented. You can also check our layout guidelines for more information.

Thanks,

Pradipta.

Thank you Pradipta.

Take care.

Ali

0 Likes