Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Hyper Flash Forum Discussions

Sort by:
ABC
Hyper Flash
Hyperflash is not responding to any commands except status register read. I tried word programming , buffer programming, sector erase, Chip erase, Dev... Show More
4867226
Hyper Flash
    hyperbus DQ wave is abnormal,why? Please help analyse。 circuit: Show More
PradiptaB_11
Hyper Flash
IntroductionInfineon’s HyperRAM can be used as an expansion memory for high performance embedded systems because it offers the industry’s highest perf... Show More
algr_4779301
Hyper Flash
Hello,When erasing S26KL512S memory sector. The data becomes FF but part of next sector is 0. When I erase the sector I wait for the flash to be ready... Show More
rozh_4786246
Hyper Flash
你好,        我们将数据backdoor到s26kl512s这个hyperflash中,然后控制ospi controller来进行读flash。在读操作之前,通过ospicontroller对flash进行复位——将flash的RESETNeg拉低,经过一段时间后释放复位,将RESETNe... Show More
ohhi_2816686
Hyper Flash
HyperFLASHおよびHyperRAMのレイアウトガイド(AN211622)の内容で教えてください。このレイアウトガイド内(4.1 章)で、「50 オームのシングルエンド インピーダンスと100 オームの差動インピーダンス (定格値) を維持しながら、CK とCK#の配線を同一平面上で行う必要が... Show More
ohhi_2816686
Hyper Flash
02モデルの使用の検討をしています。以下確認をさせてください。 ・PSC, PSC#端子は無いであっていますでしょうか? ・上記YESの場合、この端子はNCまたはDNUのどちらになるのでしょうか? ・3VデバイスのCK#も同様の認識であっていますでしょうか? Show More
ToKo_1330256
Hyper Flash
ご教示お願い致します。MPN:S71KS512SC0BHV000確認事項:・電源投入直後のデータの消去-書込み速度と電源投入後しばらくたった後での データの消去-書込み速度にバラつき(電源投入直後の速度の方が倍くらい速い)が みられるのですが、この現象について何か参考となる情報はありますでしょうか?... Show More
PriteshM_61
Hyper Flash
Do you know HyperBus Memory solution provides an optimum high-performance memory subsystem with 70% fewer pins and a 77% smaller footprint compared to... Show More
inva_4755136
Hyper Flash
how can i download spansion_tc_pkg for testbench and not able to see in my extracted verilog model folder? Show More
Forum Information

Hyper Flash

The HyperFlash NOR Flash memories Forum offers discussions on automotive advanced driver assistance systems (ADAS), automotive instrument cluster, automotive infotainment systems, and communication equipment.