Hyper Flash Forum Discussions
Hello,
I am working on S6J32xx and S6J33xx and I have to be able to distinguish between S26KL-S and S26HL-T models.
I can easily get device ID of S26KL-S, but Semper HyperFlash is different and I cannot make it work.
The rest of operations work well because they are compatible between S26KL-S and S26HL-T. I am using LLD which is supplied with official sample software.
Please, can you help me with that? I guess it must be something easy, but I am not finding any working example to get device ID from S26HL-T.
Thanks in advance
Show LessKindly explain, how Address =0x555 is converted into 24-bit Row address (i.e. 0xAA) and Column Address (i.e. 0x05).
Hi!
I am using the multichip HyperRAM + HyperFlash S71KL256 (based on S26KL256) for a custom application with STM32H725. I have succeeded setting up communications in memory mapped mode for both FLASH and RAM.
However, I am stuck on the programming for the FLASH. I am desperate in finding examples using the HAL API's functions like HAL_OSPI_HyperbusCmd etc..
Please, is there anything you could refer me to?
Many thanks in advance
Show LessPlease advise what are the product applications for S26KL512SDABHB020?
Thanks
Please provide maximum junction temperature for IC S29GL01GT11DHB020.
We require this data on urgent basis.
Hi,
I want to use S26KL128SDABHN030 memory with STM32L4+ microcontroller. I read that this memory has DCARS feature. Is it possible to disable it to use this memory without PSC signal?
Show LessI am looking to get in contact with Cypress and do a LTB for part that is above being discontinued. Infineon told me to post here to get in contact with Cypress
Show LessWhere to get the layout guideline for S26KS256SDPBHB02 ?