Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Hyper Flash Forum Discussions

Hyper Flash Forum Discussions

Sort by:
GrCa_1363456
Hyper Flash
Which hyperbus memories are recommended for NXP's i.Mx RT platform.Are Cypress' HyperFlash/HyperRAM MCP devices compatible with NXP's i.Mx RT series?A... Show More
Anonymous
Hyper Flash
Hello, I want to use S25FL116K0XMFI011 SPI Flash Memory. How can I read/write data via TMS28069 ? Is there any code example or document to guide me ? Show More
Anonymous
Hyper Flash
Hello.I plan to use HyperFlash memory with  my new iMX RT project, but I want to have a possibility to use QSPI Flash instead of it, with shared footr... Show More
toyac_1469256
Hyper Flash
Vcc:1.8V温度:-40~85℃周波数:166MHz容量:128Mb、256Mbの条件にてPSC/PSC#の端子がある製品はありますか? Datasheet上はラインナップが無いように見えます。 Show More
JuIn_1625121
Hyper Flash

Even if Future HyperFLASH and HyperRAM's capacites increase, will be these Footprint not changed?

Anonymous
Hyper Flash
HyperRAM IP
Solved
hi I am working on TE0725 TRENZ evaluation board ... I want to implement HyperRAM with vivado but there is no IP for HyperRAM so please help me how to... Show More
Anonymous
Hyper Flash
Hi,I am using K66F and KV58F MCU from NXP and I want to expand Flash and RAM.Can I use Hyperbus Flash and RAM or QSPI Flash and RAM to do so?What is r... Show More
HINA_2218186
Hyper Flash
Is there a possibility of ignition / smoke generation when the adjacent terminal is short-circuited with 10 kΩ (due to condensation etc.)? Show More
HINA_2218186
Hyper Flash
INT#端子が、書き込み/消去時のBusy状態以外でLow出力する条件があれば教えてください。【質問の背景】基板実装時にハンダの接続不良を検出する際に、データを書き換えずに検出したい為です。 Show More
Anonymous
Hyper Flash
Would be great to have the option to have two devices and fit as necessary, is this possible and and if so whats issue might I see?The bus seems to le... Show More
Forum Information

Hyper Flash

The HyperFlash NOR Flash memories Forum offers discussions on automotive advanced driver assistance systems (ADAS), automotive instrument cluster, automotive infotainment systems, and communication equipment.