Recent discussions
Thank you for your kind reply.
If our company pays for Hall Sensor(TLE49641KXTSA1), are you willing to obtain UL specifications for the product?
- UL Safety Specification Certification Certificate
If it is possible, please let us know what we should do.
Please Check. Thank you
Show LessDear all,
i'm using the TLE4959 with a pullup of 2,7kohm of Rload with 12V of supply voltage.
Is there a limit condition of growth of Rload for the correct operation of the transducer?
Thanks in advance
Claudio
Show LessI'm using an infineon TLE4941plusC hall effect sensor to measure speed of a rotating shaft. I was wondering if there was any information available on the recommended dimensions of the target wheel?
Show LessDear Community memebers,
TLE4999C8 requires a programming pulse (beside SICI communication) to store EEPROM content. On which pin of the IC do I need to apply the programming pulse? The datasheet and user manual does not contain this information.
Thanks in advance for the help!
Show LessHello.
I would need the evaluation board and GUI SW for the TLE4999C8. I did not found any information on it on TLE4999C's webpage...
(I already have PGSISI-2 and 3 boxes. I used it for TLE4997 and TLE4999i3 ).
Thank you.
Show LessHi,
we got a problem with an PGSIS-2 Box, it has telegramm response errors.
The in the original built-in box is a version 3.3.1. But we have only a version 3.5.3 in stock
So I replaced the the old one with the 3.5.3. But it dosen´t work with our software... new error: „Get2send resault_change fromPGSISI-2 Error occurred“
My Question! Is it possible to downgrade the pgisis box from 3.5.3 to 3.3.1?
thanks for your help
Show Less
I have no idea how to use SICI interface. I want to learn it. In my project, i will use TLE4993I3 hall sensor and i should learn how to use sensor in my circuit and how to pragramme it?
Show LessDear Supporter
I want to translate the following KBA. Please confirm to my work.
TLE4922 Magnetic Speed Sensor: What is the minimum air gap?
Regards,
Nino
Show LessDear Supporter
I want to translate the following KBA. Please confirm to my work.
Hidden adaptive hysteresis concept of magnetic speed sensor TLE4922
Regards,
Nino
Show Less