Recent discussions
Hi,
we got a problem with an PGSIS-2 Box, it has telegramm response errors.
The in the original built-in box is a version 3.3.1. But we have only a version 3.5.3 in stock
So I replaced the the old one with the 3.5.3. But it dosen´t work with our software... new error: „Get2send resault_change fromPGSISI-2 Error occurred“
My Question! Is it possible to downgrade the pgisis box from 3.5.3 to 3.3.1?
thanks for your help
Show Less
Dear Supporter
I want to translate the following KBA. Please confirm to my work.
TLE4922 Magnetic Speed Sensor: What is the minimum air gap?
Regards,
Nino
Show LessDear Supporter
I want to translate the following KBA. Please confirm to my work.
Hidden adaptive hysteresis concept of magnetic speed sensor TLE4922
Regards,
Nino
Show LessDear Supporter
I want to translate the following KBA. Please confirm to my work.
Can TLE4922 be used together with a magnetic encoder wheel?
Regards,
Nino
Show LessHi
I want to get the three coordinates values of the magnetic field measured by the sensor of my phone. For this, I get a handle to the SensorManager
by using sm=(SensorManager)getApplicationContext().getSystemService(Context.SENSOR_SERVICE)
, then get the sensor with cm=sm.getDefaultSensor(SensorManager.SENSOR_MAGNETIC_FIELD)
. I then register a SensorEventListener
to the SensorManager
with sm.registerListener(new SensorListener(),cm,SensorManager.SENSOR_DELAY_UI)
.
The classSensorListener
is a class of my own implementing the SensorEventListener
interface. In it's OnSensorChanged
method, I get the values from the sensor and I display them. The problem is that I only get the values 1,0 and 0. And they are rarely updated (I have put a counter on the onSensorChanged
calls to see how often the update takes place). Changing the time to SENSOR_DELAY_NORMAL
doesnot improve anything.
To check if the problem was related to the magnetic sensor, I have added, in the same way, a listener to an accelerometer sensor. The result is very confusing : now, the magnetic sensor generates updates, but not the accelerometer one. And if I remove the accelerometer omegle.2yu.co sensor event listener, I still receive the magnetic sensor events which where missing before adding the accelerometer sensor event listener.(???????????)
Any idea about what is wrong in omeglz my code?
Show LessWe changed VS Voltage 12V to 5V as a attach file that is TLV4996K_VS.
It has happened strange waveform as a attach file that low is 1.3V.
So, We tested VS has R Value(220 ohm) to 0 ohm. and then, The above phenomenon wrong waveform disappeared.
Can we use schematics it. and Can you recommend schematics?
Thanks
Best Regards
Gerald. Show Less