Recent discussions
Dear Supporter
I want to translate the following KBA. Please confirm to my work.
Can TLE4922 be used together with a magnetic encoder wheel?
Regards,
Nino
Show LessHi
I want to get the three coordinates values of the magnetic field measured by the sensor of my phone. For this, I get a handle to the SensorManager
by using sm=(SensorManager)getApplicationContext().getSystemService(Context.SENSOR_SERVICE)
, then get the sensor with cm=sm.getDefaultSensor(SensorManager.SENSOR_MAGNETIC_FIELD)
. I then register a SensorEventListener
to the SensorManager
with sm.registerListener(new SensorListener(),cm,SensorManager.SENSOR_DELAY_UI)
.
The classSensorListener
is a class of my own implementing the SensorEventListener
interface. In it's OnSensorChanged
method, I get the values from the sensor and I display them. The problem is that I only get the values 1,0 and 0. And they are rarely updated (I have put a counter on the onSensorChanged
calls to see how often the update takes place). Changing the time to SENSOR_DELAY_NORMAL
doesnot improve anything.
To check if the problem was related to the magnetic sensor, I have added, in the same way, a listener to an accelerometer sensor. The result is very confusing : now, the magnetic sensor generates updates, but not the accelerometer one. And if I remove the accelerometer omegle.2yu.co sensor event listener, I still receive the magnetic sensor events which where missing before adding the accelerometer sensor event listener.(???????????)
Any idea about what is wrong in omeglz my code?
Show LessHello,
What current and voltage can the TLE4961-1M High Precision Automotive Bipolar Hall Effect Latch resist over time on pin 2 and still be okay and functional afterwards?
BR
Show LessDear All, I'm trying to get a clear statement of which automotive grade is TLE4966-2G, but cannot find any "AEC-Qxxx" statement in datasheets, nor in other technical documents.
Can you please help ?
Thanks in advance for support
Best regards
Show LessWe changed VS Voltage 12V to 5V as a attach file that is TLV4996K_VS.
It has happened strange waveform as a attach file that low is 1.3V.
So, We tested VS has R Value(220 ohm) to 0 ohm. and then, The above phenomenon wrong waveform disappeared.
Can we use schematics it. and Can you recommend schematics?
Thanks
Best Regards
Gerald. Show Less
- « Previous
-
- 1
- 2
- Next »