Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

HEMT (GaN) Forum Discussions

HEMT (GaN) Forum Discussions

Sort by:
KUOWENYUNG
HEMT (GaN)
Dear Sir, The pulsed current capability at Vds=600V is also in that case basically null. May I know the phenomenon root cause? it's material or horizo... Show More
Lucaris7
HEMT (GaN)
I want to use CoolGaN™ 600 V half-bridge evaluation platform featuring GaN EiceDRIVER™. However, this board expects a 50ohm pulse generator. I wonder... Show More
Lucaris7
HEMT (GaN)
I  want to buy the pluggable wire connector, which can be connected with the EVAL_1EDF_G1B_HB_GAN board. Anybody can tell me? Show More
QQdonald
HEMT (GaN)
When I download its simulation model  from website and use it in LTspice,it shows unreadable code in this file,how do I fix this problem?  Show More
dk_y
HEMT (GaN)
Hi, i am using IGT60R070D1 for boost pfc converter. I am trying to estimate the power losses (switching and conduction losses) before make the system.... Show More
Miyata
HEMT (GaN)
My customer want to know the IGT60R070D1's VGS max value.  If I look into the data sheet, these is no value specified.  Competitor GaN System has a si... Show More
User19220
HEMT (GaN)
Hi,I want the 3D models(step files) of the following devices - 1. IGOT60R070D12. IGT60R070D13. 1EDF5673KThese 3D models are unavailable on the website Show More
User19220
HEMT (GaN)
Hi,Is it ok to connect NC pads to either of Drain, Source terminals? In the layout, due to the NC pins being adjacent to the Drain pins, the drain cop... Show More
Mausraus
HEMT (GaN)
GaN switch
Solved

Are you also offering  GaN switches in 600V

Forum Information

HEMT (GaN)

Infineon’s CoolGaN™ is a highly efficient GaN (gallium nitride) transistor technology for power conversion in the voltage range up to 600V. The pioneering quality ensures the highest standards and offers the most reliable and performing solution among all GaN HEMTs on the market. Switched-mode power circuits using CoolGaN™ can benefit from the improved energy efficiency and the improved power density, which is not possible with state-of-the-art silicon devices. In this forum, you can post your questions, comments, and feedback about CoolGaN™ devices and their applications.